Hi, I'd need some clarification about the SOH update available on the BQ34Z100 on a lead-acid battery.
This post [https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/993404/bq34z100-maintenance-cycle-to-update-soh/3669498] seems to tell that we need to discharge the lead-acid battery of 37% to update the SOH.
However this other post [
https://e2e.ti.com/support/power-management/f/power-management-forum/714383/bq34z100-g1-minimum-requirements-for-soh-update] seems to tell that the SOH is not linked to the SoC, but to the FCC Update.
Question 1 : What information is the right one? In other words, can I get (precise value or not) a SOH estimate if my battery oscillates only between 100% SoC and and 80% SoC in normal operation ? What about less than that ?
Also, in the slua450 it is written that "In order to ensure high accuracy of the DOD measurement, the Qmax calculation does not occur if the temperature is above 40 or below 10. Il also does not occur if at least one of voltage measurement for DOD1 or DOD2 was taken in the cell voltage range between 3737 mV and 3800mV because of very flat OCV(DOD) dependence in this range." and then that "These limits are chemistry dependant and are specified for different chemistries separately" and then that "Qmax is calculated as Qmax = PassedCharge / (DOD2-DOD1)".
Question 2 : Considering this, can I know these limits for my lead-acid battery chemistry? It is certainly different from the one specified in the slua450 since the OCV curve of a lead-acid battery is definitely different from a lithium-ion battery and their performances in temperature is also different.
Thank you