Please let me know if you can confirm these details from the datasheet-
- Page 1 refers to the ‘MODE pin’ for selecting between PSM & FCC modes. Is the MODE pin also multiplexed with this function, or is this just a typo that should be referring to the PSM pin?
- The table on Page 19 lists “Connect to high or float” for some rows of the ‘MODE’ pin in the “Automatic Power Sequencing” section, however elsewhere “Floating” is defined for “Externally Controlled Sequencing”. If the former half the piece that is incorrect?
If these were typos can you clarify?
Thanks!