This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM73606: Startup Time after Enable

Part Number: LM73606


Figures 65-68 of the datasheet appear to show a delay (approximately 800 us) between the EN pin going high and the start of the ramp on the output (see image below). However, the Soft Start timing characteristics in section 6.6 of the datasheet indicate that the soft-start time starts on the rising edge of the EN pin. Is there an internal delay between the rising edge of the EN pin and the control logic starting to switch the high side FET?