Part Number: BQ78350-R2-DEVICE-FW
Hello I have a question regarding the BQ78350_R1 with the software R2 downloaded in the chip.
When I apply a short circuit and I have:
Setup the protection ASCD with a latch limit to 5, Counter DEC Delay to 3,Recovery to 1, Reset to 5.
PRotection configuation bit DIS_AFEtime_RECOV is set.
Setup the settings Enabled Protections A ASCDL to 1 and ASCD to 0.
The systems keep on repeating after the inetervals to start over again for ever.
Setup the settings Enabled Protections A ASCDL to 1 and ASCD to 1.
The systems switch of when ther is a short and will not turn on automaticly, only when short is removed and charger is applied.
I have tried a lot of combenations and settings and the system keep on reseting or get stuck and can not start the system again when the charger is aplyed again after removing the short.
What I'm looking for a setting that when the system is seeing a short the DSG fet will be turned off. after a second it should start over again and when the short is still there again the DSG FET should be switched off. This should be repeatred upto the latch limit in my case 5 times then it should stop trying forever until the short is removed and a charger is aplied and BMS should be switching on the DSG FET.
I whant to use this for havy load with a high inrush current.