This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63020 inductor selection for high output current

Other Parts Discussed in Thread: TPS63020

Hello,

I would like to know how to choose an inductor for the TPS63020 converter.  My application will require 4.5V @ 1.5A output, boosting from a li-ion battery (2.7V to 4.2V input).

The datasheet for the TPS63020 provides the following equation for determining inducator value (boost mode operation):

L = 0.5 x Vout

For my application, this means I would need at least 2.25uH to boost from 4.5V.  However, the equation doesn't seem to take into account output current or input voltage.  Given that I need 1.5A on the output, would I need to increase the inductance value to to achieve the required output current?

Thanks in advance,

Daniel

  • Hi Daniel,

     

    In your case you will use this equation to calculate the inductor Value:

    L=Vout/2

     

    The peak current for the inductor in steady state operation can be calculated using equations 4 and 5 from datasheet (TPS63020) on page 16. In these equations the input voltage and the output current are taken in consideration.

     

    I based my calculations on a minimum frequency of 2.2MHz and I found

     

    I1=1.8425A

    I2=3.2341A

     

    The critical current value for selecting the right inductor is the higher value of I1 and I2 which is the 3.25A.

     

    Thanks!

    Tahar Allag

  • That's exactly the answer I needed.

    Thank you for the help!