Hi,
Is TPS74601 the same characteristic as TPS74618-Q1 almost when output voltage set 1.8V?
Best Regards,
Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is TPS74601 the same characteristic as TPS74618-Q1 almost when output voltage set 1.8V?
Best Regards,
Kuramochi
Hi Kuramochi-san,
Yes the devices will be have the same, just keep in mind the external resistor divider used to set the output of the adjustable version will contribute a small amount of inaccuracy when compared to the fixed voltage device. This is because the fixed voltage device has the resistors internal which provides very good resistor matching, but ultimately this is a minor difference.
-Kyle