This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561: Enabling/disabling interrupts (INT) pin in runtime

Part Number: BQ27Z561

Hi,

Is it possible to temporarily disable the interrupts raised on the INT pin during the normal operation of the Fuel Gauge?

I can see no standard nor manufacturer command that could do that, so I guess I need to write 0 to the IO Config[INT_EN] Flash register. Unseal of the Gauge is required here. Is the reset also required to IO Config[INT_EN] 0 write take an effect?

Best regards,
Wojciech Winnik