This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2061C: Device with Similar Performance/Functionality to MAX8586 1.2A USB Switch

Part Number: TPS2061C
Other Parts Discussed in Thread: TPS2051B, TPS2553

Hey team,

I am looking for a TI device with similar performance/functionality to the MAX8586 Single 1.2A USB Switch with programmable current limit in 3mm x 3mm TDFN

The device has the following characteristics:

MAX8586

Current Limit (mA)

500-1200

# Power Switches

1

USB

Yes

Fault Indicator

Yes

Current Limit Accuracy (%)

14

Current Limit Set by

Resistor

Lowest Adj. Setting (A)

0.5

RON (Ω) (typ)

0.055

VSUPPLY (V) (min)

2.7

VSUPPLY (V) (max)

5.5

Oper. Temp. (°C)

-40 to +85

Package/Pins

TDFN/8

Budgetary
Price (See Notes)

0.66

VSUPPLY (V) (min)

2.7

The TPS2051B appears to be a device with similar performance and functionality, however, there was also a thread here that referenced the TPS25944 as a potential replacement as well, although this thread is quite dated.

Is the TPS25944 still the recommended device with closest functionality or would the TPS2051B or a similar device be a better fit?

Thanks,

Austin Allen