Part Number: BQ24618
Other Parts Discussed in Thread: BQ24610, BQ24600, BQ24610EVM
Hello TI,
I am currently designing a battery management system. All parts are functional and it includes a 6 cell pack (4P-6S) (3500mAH cells) total voltage of 25.2 when fully charged. It has a MCU, coulomb counter, third chip that has 14 bit ADC, SOC LEDS, balancing circuit, and a bidirectional switch to turn off charge and discharge when needed. The current design does not have a charger built into the schematic/PCB. I am wondering two things:
2) Does TI foresee any problems if the bq24618/bq24600/bq24610 charging circuit is external to this? I am planning on building this charger separate and connecting it to the top cell and ground of the other BMS PCB. My other circuit can handle balancing the cells and cutting off charge during overvoltage situation. I am planning on using the max charger current of around 10A.
3) With a charger voltage input max of 26V, can the BQ24618 charge a 25.2V battery? I saw somewhere in the datasheet that a higher voltage might be recommended.
Thank you for your help.