There's confusion regarding cell balancing in Relax mode vs. Sleep mode:
If I enable Sleep mode, but disable balancing while in Sleep mode, it seems that I can no longer balance cells? is that correct.? If Sleep mode is enabled, the device will transition from Relax mode to Sleep mode when indicated...and so if I have disabled balancing during sleep, it appears that balancing will effectively be disabled???
..also, it appears that even after I disable that bit (bit2, CB_SLEEP) and reset the 952, Studio shows that cell balancing continues??? What else must I do to stop balancing in Sleep mode?