Other Parts Discussed in Thread: TPS55340, TPS61088, TPS61288
Hi,
I am going to add a boost regulator to generate 12V output from single cell battery (Vmin = 2.7V, Vmax = 4.2 (fully charged) ) and our current requirement is 2A continuous current. As per the We Bench when I enter the values for TPS55340-Q1 then it is not showing any design and asking to alter the value with reducing the Iout to 1A works.
Can you please confirm if we can use this regulator to generate 2A or in other case any other solution that you can sugget?
Kind regards,
Muhammad Awais