Hi all,
I am not able to be clear about the selection of SMPS topology and corresponding controller IC for my application. The requirements for my application are:
1.) Isolation required
2.) Input voltage range - 300V to 800V
3.) Power required - 150W
4.) No of output - 24V/6A and ±15V/100mA
5.) Efficiency - not to critical (as SMPS is used for supply of other larger power rated circuits)
6.) Cost and assembly - critical (as required in large number)
7.) Radiation issues - critical (if we opt for fixed frequency operation)
8.) Size - not critical
Please give me some suggestion or source to be clear about it.
Thanks,
HS