Hi
Please suggest Feedforward Cap needs much?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
A feed forward capacitor from VOUT to RSP is design to bypass the feedback divider and change the attenuation factor from VREF/VOUT to 1/1 at high frequency in order to improve bandwidth and phase margin at cross-over. In this case, with the feedback divider ratio so small (1 / 1.2) the boost in phase and gain will be quite small and may not be worthwhile.
With your existing Cramp selection and output capacitor configuration, I would not recommend a feed-forward capacitor. If you were going to lower the bandwidth by changing the Rramp from Open to 187kΩ then I would recommend adding a feedforward capacitor sized to provide a 55kHz cross-over with the 2kΩ Vout to RSP resistor. that would be 1.5nF.
I entered the design into the attached design spreadsheet to evaluate the loop to find the approximate cross-over frequency. Without the feed forward capacitor and selecting the smallest ramp (largest Cramp value) I estimated the crossover frequency well above 100kHz, with the added boost of the feed-forward divider, I am concerned the bandwidth could get too high and unmodeled parasitic delays in the power delivery path could degrade the loop phase margin and stability.
Loop bandwidths over 100kHz or 1/5 of the switching frequency can get tricky as propagation delays and board parasitics start to additional poles into the loop and degrade phase margin, but a typically target cross-over is between 1/10 and 1/5 of the switching frequency.