Other Parts Discussed in Thread: TPS568230,
Hi support team,
Please let me know differences between TPS568230 and TPS51396A.
I think there are the following, are these correct?
TPS568230 TPS51396A
VIN(MAX) 18V 24V
Forced CCM Yes No
Hiccup protection Yes No
Latch off protection No Yes
IVIN(TYP) 105uA 90uA
VENH(TYP) 1.31V 1.2V
VENL(MIN) 0.95V 0.8V
VENL(TYP) 1.11V 1.05V
Please let me know if there are others.
Regards,
Dice-K