Hi Power Management Gurus
A previous post of mine on the BQ24075 refers. The only way I managed to solve the problem was by connecting a 10k resistor between NTC and the supply. See schematic below:-
I am now challenged with a new issue, and wonder if anyone can assist. The battery charges up to 100% and then obviously stops as expected. My application draws about 100mA in a certain mode from the battery. The charger does not seem to turn on unless the USB is removed and re-inserted. Is there a way to kick start the charge without having to remove the USB?