Hi team,
Could you give me estimation on maximum collector current at following condition? Is it correct that the customer can refer to Figure 5 in NS package?
<Condition>
Ta=60Cmax
N=2, Duty cycle=100%
NS package
The Figure 5 shows about 300mA as maximum corrector current at N=2, 100% duty, at Ta=85C. So, they want to confirm if the Ta difference between Ta=85C in the datasheet and Ta=60C in the customer's system can provide larger drive current more than 300mA. If so, the customer wants to estimate how large maximum current more than 300mA at lower Ta condition (85C -> 60C).
Or if TI has any maximum collector current vs duty cycle graphs with different Ta other than 85C, could you share it with me for the customer to estimate the maximum collector current?
Best regards,
Takeshi Sasaki