This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B7702-Q1: >400mA Iout

Part Number: TPS7B7702-Q1
Other Parts Discussed in Thread: TPS7B86-Q1

Hi team,

May I ask that do we have the device like TPS7B7702-Q1 but the Iout(MAX)>400mA?

The customer want to choose a device integrated protection and diagnostics and can support:

Iout(MAX)>400mA.

VIN(MAX)>35V

Adjustable output: 5-16V.

Dual channel or four channel is better,

Seems like TPS7B86-Q1 can meet the voltage and current requirement, but it's not integrated the protection and diagnostics function.

Do you have any recommend?

Thank you!

Regards,

Ivy