This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51561-Q1: Multi-phase Boost Configuration

Part Number: LM51561-Q1
Other Parts Discussed in Thread: LM51561,

LM51561 seems to have some interesting features regarding Dual Random Spread Spectrum and external sync.

However I noticed that if external sync signal is fed, the feature will be disabled. Therefore I have following questions.

1. Can multiple LM51561-Q1 running  in parallel with dual random spread spectrum enabled? Any potential risks?

2. Can LM51561-Q1 accept external clock with jitters or variable frequency clock? 

Thanks,

  • Hello Hua,

    1. Multiple LM51561 can run in parallel with DRSS enabled. They will not operate at the same frequency and you might observe some increase in the low frequencies that you use for DRSS.

    2. Yes, it can accept external clock with jitter.

    Best regards,
    Brigitte

  • Hello Hua,

    did this answer give you all the required information. If yes, it would be great to click the resolved button.

    Thanks,

     Stefan

  • Hi Hua,

    I’m assuming you were able to resolve your issue. If this isn’t the case, please click the "This did NOT resolve my issue" button and reply to this thread with more information. If this thread locks, please click the "Ask a related question" button and in the new thread describe the current status of your issue and any additional details you may have to assist us in helping to solve your issues.

    Regards,

     Stefan