This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: BQ40Z50R1-MAX ERROR

Part Number: BQ40Z50-R1


Hi 

I have designed a 4S1P battery pack with BQ40z50-R1 IC

I have completed the learning cycle for the battery pack and put the battery pack under long run testing ( i.e continuous charging and discharging)

From the testing the battery behaviour is found to be normal.

During the start of the testing the Max Error is 1%,Now the Battery has completed almost 50 cycles  the maximum error has now changed to 3%.

Will that affect the battery life cycle?, Why there is change in Max Error ??

Let me know the suggestions

Regards

ANANDAN