Other Parts Discussed in Thread: GPCCHEM, BQ40Z50, BQSTUDIO
I just brought up a new 2S1P pack with BQ40Z50R2, 4500_2_11, ChemID 2591.
I went through all the settings I am aware of, the pack seems to be functional, but the pack voltage shows 6983mV at 100% which is off since I know the battery is at about 45%, and the voltage is too low for 100%. Which register do I need to set for the true SoC to show? Going through a discharge does not show the change in the SoC.
Thanks,