This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EV2300-084: The EV2300 connection could not be initiated

Part Number: EV2300-084
Other Parts Discussed in Thread: EV2400, BQ40Z50, BQEVSW

Dear All,

I am trying to use EV2300 on windows 10 in Bq Evalution software  bqEVSWSetup00.09.59_bq20z95v1.50_bqEasy1.85.exe. But at staring it shows this message and unknown devices in windows devices manager.

I already tried this link for USB driver. e2e.ti.com/.../ev2300-is-ev2300-driver-available-for-windows-10-64-bit

And also I am aware that this is an old devices But these are available to us and we do not have time to buy and switch to the EV2400. I need to connect a BMS board we designed with Bq20z95. I am using Windows 10 64 Bit. If any one has gone through same problem and find solution Please Help.

Regards,
Aman