This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51397A: Differences from TPS56C230

Part Number: TPS51397A
Other Parts Discussed in Thread: TPS56C230,

Hi support team,
Please let me know differences between TPS56C230 and TPS51397A.

I think representative differences are as follows, are these correct?

  TPS56C230 TPS51397A
VIN(MAX) 18V 24V
IOUT(MAX) 12A 10A
IOCL(TYP) 15A 12A
INOCL(TYP) 4A 3.2A
RθJA 42.3℃/W 49.7℃/W
IVIN(TYP) 400μA 110μA
FCCM Yes No
OOA No Yes
Frequency 500kHz 500kHz, 800kHz
Hiccup protection Yes No
Latch-off protection No Yes

In addition, I think there is the following.

  • ABS and ROC of VIN, BST, SW terminals.
  • Each value of Thermal Information.
  • MIN and MAX of IOCL.
  • Conversion efficiency.

Please let me know if there are others.

Regards,
Dice-K