This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65296: Please help to check the design, thanks

Part Number: TPS65296

Dear sir,

Please help to check if the schematics design is ok or not, thanks!

PVIN = 12V

PVIN_VDD1 =  5V

Load: Micron LPDDR4 4GByte * 2pcs

This PMIC is design for the power supply of LPDDR4 , so we don't need the LDO channel, my doubt is if we can let the LDO input(VLDOIN) float?

Appreciate your great support, thanks!