Other Parts Discussed in Thread: BQ24179, , BQ25792
Hi,
We are planning to charge the battery pack 12.6V max , 2600 mAH via Type C input source (5V, 1-2A), Please Suggest the Suitable Charging controller with out I2C interface for our requirement.
please suggest the suitable controller for our requirement,
As discussed with Jonard Rico, they suggested BQ24179 IC for with out host control It can operate the buck boost configuration,based on the input source.
If its possible please share the example circuit for the same.