Can LP87523 be used instead of LP87524? (LP87524 out of stock).
Can the LP87523 chip (3 output) be configured to be a 4 output power chip by using IIC communication? If possible, which parameters need to be configured?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can LP87523 be used instead of LP87524? (LP87524 out of stock).
Can the LP87523 chip (3 output) be configured to be a 4 output power chip by using IIC communication? If possible, which parameters need to be configured?
Hello Liu,
Unfortunately it is not possible to reconfigure the phase setup through I2C command.
Thanks.
Regards,
Tomi Koskela