This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2901-EP: Using the UC2901-EP as an unregulated DC/DC converter module

Part Number: UC2901-EP
Other Parts Discussed in Thread: DCP020503

Hello:

I have used the DCP02 Series, 2-W, 1000-VRMS Isolated, Unregulated DC/DC Converter Modules for bias supplies for H=bridge circuit.

I have an application where I need an extended temperature range (-50C)  DC/DC converter. Vout=12-15VDC at 50mA-100mA . 

1. Is there an extended temperature (EP) parts for the DCP02 series DC/DC converter?

2. Can I run the UC2901-EP open loop with a transformer isolated output?

3. Is there a better TI solution that you can recommend to make a 15VDC bias supply @ 50mA-100mA that operates down to a temperature of  -50C 

4. If the UC2901-EP ic is a good candidate for my bias supply are there pre-designed isolation transformers that work with the UC2901-EP.

Thank you for your help,

Jim