This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H1101A-SP: Output Trys to Turn on When Enable Is LOW

Part Number: TPS7H1101A-SP

When enable pin is HIGH, Vout = 3.3V which matches our design, everything is good. However, when we force enable pin to ground, after we turn on the power Vin = 5V, we get Vout = 2.1V. We have CS pin has been pull HIGH to 5V through 110K ohm, is this the reason why Vout trys to turn on when enable is LOW?