Hi,
Good day.
Our customer is evaluating the BQ25790EVM and they have the following question.
""I am currently doing some evaluation on the chip and wanted to ask can the chip automatically terminate discharge or shutdown when the battery is low :
case if a 4 cell battery (16.8Vmax) is attached to the IC charger and the safe lowest discharge voltage for the 4 cell is 12 V. will the IC charger shutdown automatically at 12V or do I need a microcontroller to use the I2C to manually shut it down?""
Looking forward to your inputs. Thank you.
Regards,
Cedrick