Hello,
I am looking to use a custom cell with the BQ40Z50-R3 and wanted to make sure that I understand the process for this. As far as I can tell, I should do the following:
- Run the procedure outlined in “slva725a.pdf” (run a cycle on the cell, format the data correctly, upload it to TI, and the automated system responds with the best match; program the gauge with this).
- Run the procedure outlined in “sluubd0.pdf” (run a cycle on the cell at room temperature, then cold temperature, format the data correctly, upload it to TI, and the automated system responds with values to adjust in the gauge to handle low-temperature behavior; update the gauge accordingly).
- Run the procedure described in “slua848.pdf” to do a learning cycle on the full pack (again, running a cycle that includes some rest periods, while commanding the gauge at certain points).
I had some questions about the first two steps here:
- Is it ok to run Steps 1 and 2 using a bare cell on a Maccor? Step 2 recommends the final product (which will not be available yet) or attempting to replicate the thermal conditions better (putting the cell in a case to mimic the thermal properties of the final battery).
- Low temperature performance is important for my project (all the way down to -30C). Is it possible to run it at multiple temperatures and combine the optimization results? If not, how should I select the low temperature to test at?
- What if there is not a good match for step 1 above?
- Is there any way to refine the gauge’s behavior if it does not meet the customer’s accuracy requirements?
- If this process does not work well for my application, what is the method to get a cell added to the list of cells that the gauge supports?
- Can I adjust the gauge to be more pessimistic about SOC? (i.e., always try to err on reporting less energy is available, rather than over-estimating?)
Thanks,
-Eric Castle