Hello,
My customer has a couple of questions about LM5067 as follows
Q1:
The Itimer (Insertion time current) variation in the data sheet is large, from -9.5uA to -2.5uA.
They would like to consider the temperature environment and other factors to determine the appropriate variation.
Is there a temperature characteristic graph for Insertion time current?
Q2:
They understand that after calculating Ton as the processing time at startup, it is necessary to set the FaultTimeout to a value greater than this time.
The fault timer current source (85uA), which is used to calculate the fault Timeout, is described in 9.2.2.6.2. Is there any variation or temperature characteristics of the fault timer current source?
Best regards,
K.Hirano