I was curious to know what the effects were on the LM5576 regulator (if any noticeable) if the CRamp pin was either open without a Cramp cap on it or shorted to ground?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I was curious to know what the effects were on the LM5576 regulator (if any noticeable) if the CRamp pin was either open without a Cramp cap on it or shorted to ground?
Hi Jason,
I will need to check with the design team to see if they have this data. I will let you know what I find out.
Regards, Jason
Hi Jason,
The ramp pin FMEA data is shown below for the LM5576. Hope this is what you are looking for. Let me know if you have other questions.
Regards, Jason
Pin | |||||
Number | Name | Connection | Damage | Functionality | Comments |
9 | RAMP | Short to GND | No | No | OUT=1Vpk-pk oscillations around the expected regulation voltage & erratic switching |
Open | No | No | OUT=0, no switching |
Hello Jason,
Thanks for the information. Based off of what you provided I went ahead and setup my circuit to have pin 9 "open" and the regulator output is showing the correct regulated voltage out "unloaded". The information states that the output should be = 0V. Is this worded incorrectly?
For my testing, once I apply 20mA of load, the voltage does drop a bit. I can add another 20mA load and it drops it a bit more. If I increase the load to 500mA it drops the output voltage significantly.
Just curious for some clarification.
Thanks,
Jason
Hi Jason,
Not sure, but this may have been tested at full load. I expect VOUT = 0V if no C_RAMP is added. Can you add a C_RAMP and check the behavior?
Regards, Jason