Hi,
We designed and developed a charger based on BQ24616. It is not charging the battery even though the conditions are met.
Vfb - 2.065 V
Vts - 1.89 V - 57% of Vref
VISET1 - 820mv, RSR - 0.01E so ISET1 = 4.1A
VISET2 - 620mv so ISET2 = 3A
VACSET = 320mv, RAC - 0.01E so ACSET = 1.6
CE - High
These things are working fine:-
PG LED glows
STAT1 Glows when Vfb < 2.1 V
STAT2 Glows when Vfb > 2.1 V
REGN - 6V
VREF - 3.3V
BATDRV and ACDRV works fine when AC power connected and removed.
Issue - Device not charging the battery.
I have changed the Resistor divider in FB and TS section in the schematic to meet the conditions. Values in the schematic are updated.