Hello,
I have tried to send the commands via command section on the GUI to change settings of ICs such number of Cells, Auxs etc. but the probelm is I do not see those changes on the GUI interface where all data are shown. is it because of GUI program does not allow us to change the ticked sections such as Cells number and Auxs?
so I do want to see the changes that I would like to make with GUI to understand sequence of code. can you tell me how to make revision with send command part in GUI
the second question is I tried to set the Comparator threshold values like OV and UV to 4.2V and 2.8V respectively but the values automatically get down to 4V and 2V respectively can you tell me what that cause to happen? you can see in the picture below with more details
.