This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25119: Consultation

Part Number: LM25119
Other Parts Discussed in Thread: LM5143-Q1

Hi TI

We are designing a power supply for motor drivers, the system is requiring up to 24V/35A.

We have selected LM25119 to regulate input voltage (26-30V) to 24V.

  • Is it possible to achieve these requirements by a single channel or we have to use the interleaved single output?
  • This part isn't supported by WEBENCH is there any other method to get the calculations needed.
  • Is there any evaluation that has the same (or close) to our requirements?
  • Can you review the schematic design after I finish it?

Thanks