Hi Team,
We heard from my customer that when look into detail start up waveform of TLV707/742, they found that there will be an over spike at Vout. Please find below schematic and waveforms for TLV70712.
The input voltage is 3.3V, EN pull up to Vin, since this engineer only have 2 probes, they have to separate 3 channels in 3 images. All CH1s are 1.2Vout, you can see the maximum value is 1.35V.
I have asked them to make 3.3Vin stable and flip the EN from low to high, the test result remained same. They have tested on several boards with same phenomenon. While WILL Semi has no such kind of issue(see attached 韦尔)
Could you please double check on our EVM with the same setting? The output current is hard to test since connected with the on board load. I will try to let them double confirm with no load and a CR load. Thanks.
BR,
Rory