Other Parts Discussed in Thread: LM61460
Dear Expert ,
Good day!
Our customer need a power device which require the follow items:
input voltage: 15v up to 24v. from noisy sources, cheap power bricks...etc. OR from Meanwell power modules (180mV ripple).
output voltage: 12v (and can go down)
output current: +5 amps.
total ripple+noise at full load output: < 1 mV.
I had check our products , I found 10 device which can fulfill the first 3 requirements .Here is the link
But for the total ripple+noise at full load output: < 1 mV. I am not sure about it , I only find the LM61460-Q1 description it have the low-noise characters
1.Could you help me to confirm whether LM61460-Q1 can fulfill the requirements ?
2.what about the products in the list?
3. if the device need the ferrite bead filter , do you have any suggestion or reference design for it ?
BR,
Leon.liu