This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Uc3825 has the minimum duty cycle limit, such as 5%. If the duty cycle is less than 5%, the duty ratio of the chip output may become 0. I want to know the principle.
Hi,
The PWM is produced by comparing the ramp and the ref. When the ref is < RAMP bottom, there will be no pulses present so to become zero duty. In theory, the duty should be ok to be < 5% become jump to 0%. But in practice on reason 0 < duty < 5% may not be achieved, because propagation delay, the ref and the ramp noise, the comparator input offset needed, are all among why. UC3825 is an old device so 5% is already very good.
A newer device may have better min duty on the improvement to the mentioned,
Hi,
Different RT and CT give different speed and noise level which interact with the mentioned factors. So different min duty can be resulted.