This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24630: can or not support the 7 Cells /29.4V?

Part Number: BQ24630

Hi Sirs,

May I know the BQ24630 can or not support the 7 Cells/29.4V (NCR18650GA, 4.2V/cell)?

Why the datasheet shown the maximum charge voltage only support to 26V?

If it cannot, please advise the correct device. Thanks!

  • Hello,

    This charger is intended for Lithium Phosphate batteries which have a charged voltage of 3.6 V. With 7 cells at 3.6 V/cell the charge voltage would be 25.2 V and would be within the range.

    I will be updating the cell voltage in the datasheet for the next datasheet update.

    Thanks,

    Mike Emanuel

    Please click "Resolved" if this answered your question.