Other Parts Discussed in Thread: BQ24640
I want to know if the BQ77915 will manage LIC supercapacitors - 5 in series configuration. I plan on using BQ24640 CICV charger and limiting charge current to charge the cap stack but need to ensure balancing is maintained during the charge cycle. I also plan on using load switches in the charge/discharge modes of the application. As you will know, the LICs are rated 3.8v max discharging to 2.5v min so the stack will drop from 19v when charged to 12.5v min when discharged. I'd like some feedback before ordering the EVM. Thanks.