When BQ25611D is charged at 1A and discharged at 1A, the surface temperature of the chip is as high as 79 degrees.
1.Where is the main source of heat?
2. How can we solve it?
3. What information do we need to provide?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When BQ25611D is charged at 1A and discharged at 1A, the surface temperature of the chip is as high as 79 degrees.
1.Where is the main source of heat?
2. How can we solve it?
3. What information do we need to provide?
Hello River,
Can you share your layout and schematic? The charger needs heat sinking into the PCB otherwise it may heat up to high temperatures like you're seeing.
Sincerely,
Wyatt Keller