This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55165-Q1: TPS55165-Q1

Part Number: TPS55165-Q1

Hi Team,

I 'm designing the Buck-Boost with TPS55165. Vin:10-36V , Vout:12V , Iout: 400mA.

I analyzed the demoboard TPS55165-EVM.

I ask you if the input capacitors and otuput capacitors instead of 10uF 50V (2xCin and 2xCout),I can use 4xCin 4.7uF 50V and 4xCin 4.7uF 50V or 8xCin 2.2uF 50V and 8xCout 2.2uF 50V,

always respecting ESR<100mOhm (as prescribed in the datasheet).

Then, the Input and Output Capacitors can be Paralallelized?

Do you think there are problems about  the operation of product?

Please,let me Know.Thanks.