Other Parts Discussed in Thread: LM5163,
I was starting this conversation with the next parameters : Provide case details or comments: I'm looking to a DC/DCconvertor that can do 90VDC input and 12VDC output and low EMI and low quicient current. I found the device LM5163 I think that is a good device voor the job. i only need 12V out 20mA to 100mA is more then needed and input is 90VDC low EMC would be nice and Qicient current low is prefered. It will be a new designan for the first badge i need 50 pieces. its a new design so it must have reliable delivery when i need more parts.
Then I saw that the divice was not availble out of stock so custum support advice the device LM5164 but also this device is out of stock. and was telling me to start this conversation on this forum.
So can you help me on this one?
Kind regards
Rens