Hello,
I was planning on using the BQ24610 to charge a 4S18P Li-Ion battery pack. The maximum listed charging current for this IC module is 10A, so the charging current per series connection for my application would be approximately 10/18 A (0.56 A). Using the specifications and design guide from the data sheet, I was able to conclude that I could achieve a 10A (0.56 A per cell) charge current and 5.4A termination current (0.3A) per cell by adjusting the sense resistor RSR to 3.7 milliohms and matching the impedances of the traces back to the sense pins with appropriate VISET1 and VISET2 values. My question then becomes: Are there any pitfalls (not safety related) for an approach to charge a 4S18P Li-Ion battery with only one battery charger? Moreover, will issues arise when using only 0.56A to charge a cell with a cutoff current at 0.3A, maybe due to a combination of noise and resolution in the sense comparator for the system? One alternative I considered was to use multiple chargers (assuming sufficient input power) with relays to disconnect the battery packs; however, I dislike this approach because I estimate a power loss of around 10 to 20 watts during discharge because of the efficiency of a relay. Ergo, if I cannot use one charge to charge 18 of these battery packs in parallel, what is the limiting factor for the maximum amount of battery packs that I can charge in parallel for this particular integrated circuit?
Thank you in advanced for your time and patience