Other Parts Discussed in Thread: TPS25980
Hi TI Expert,
Currently we're using TPS26630RGER chip at automotive application.
Our customer give us the sensor power spec is Vin: 12V max amp: 5.5A
We have some questions that
1. Does TPS26630RGER withstand 6A 30ms without cutoff?
2. Could we ensure that TPS26630RGER does not cutoff when occurring 6A @10V even we change the dVdT cap to 0.1uF?
Please help to review our schematic again, and could you suggestion us another higher power limit(>6A) chip with pin2pin as backup solution?
thanks
Smith