This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62110: directly compatible with TPS62110-Q1 or TPS62110-EP?

Part Number: TPS62110


Hello,

our supplier is using the TPS62110RSA at the moment.  Because of delivery problems they want to replace it with a TPS62110QRSARQ1 which is the Q1 type or TPS62110MRSAREP which is the EP type. From the datasheet I can see they are almost indentical. In most cases the Q1 and EP types have more reserve.

Are they identical and only pre-sorted or are they physically different?

Can they be replaced directly or have we to do additional testing?

Best regards

Peter Bitz