This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5569: Maximum value of pull-up resistor in CLK pin when set as CLK master

Part Number: LP5569

Hi there,

I'm working with more than one LP5569, and want to synchronize them setting the CLK of one of the drivers as output + adding a pull-up resistor. 

My device has a low power budget, what makes me think in minimizing the current consumption on such resistor. 

Is there a maximum recommended value for this component? The 6.04k resistor of the EVM seems somehow too small for our use case.

Thanks for helping,

Bruno