This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25710: trigger IDPM in PTM

Part Number: BQ25710

Hi All,

May I know when BQ25710 is in PTM mode.

If the IDPM is trigger, will it switch back to PWM mode?

I'm not sure whether IDPM is one of the Fault condition.

Thank you for your help. 

 

  • Hi Wang,

    Thanks for reaching out.

    I did some testing on the EVM. The power stage will switch if you limit the input (IINDPM) while keeping the load the same. The supply will provide the amount of power it can to the system load with the rest coming from the battery.

    If you have no load on system but initiate charge in PTM mode, power stage will switch as well.

    We have the EVM for evaluation if you or your customer is interested.

    https://www.ti.com/tool/BQ25710EVM-017 

    Thanks,

    Peng

    *If my answer solves your question, please press "This Resolved My Issue" on the thread.