This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS709: ABS or ROC of NC terminal

Part Number: TPS709

Hi support team,

It is said that it is okay to connect the NC terminal to another net, but is it okay to supply 28V?

Please let me know if you have Absolute Maximum Ratings or Recommended Operating Conditions.

Regards,
Dice-K

  • Hello Dice-K,

    These pins are not internally connected so you can tie 28V to them if you would like.  You will want to be sure you follow the proper conductor spacing guidelines in your application.  Please ensure that the conductor spacing from the NC pin to the adjacent pins is sufficient for 28V, such that no arcing may occur in your product.

    Thanks,

    - Stephen