This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: Chip Consultation

Part Number: BQ25792
Other Parts Discussed in Thread: BQ25730, BQ25731, USB-PD-CHG-EVM-01

Hi Team,

I want to find a charger chip can support PD(Buck-Boost) plan. The charger needs to be PD fast charging to battery(7.4V@4900mAh). What's more, it should support charging with both 5V and 12V adapter. BQ25792 may can meet the requirements. What others are suitable for this case?

Best Regards

Gust

  • Dear Gust,

    If you would like to use a charge controller, the BQ25730 and BQ25731 are also viable options (BQ25730 has power path and BQ25731 doesn't). If you want to use the BQ25792 I would recommend looking at the reference design USB-PD-CHG-EVM-01 which combines the PD controller and the battery charger.

    Thanks,

    Mike Emanuel

    Please click "Resolved" if this answered your question.