This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: learning cycle fails update status not changing to 06

Part Number: BQ34Z100-G1

Hello team, the Learning cycle fails. 

I understand that one off the main condition to end a Learning cycle is to have at list 90% of DOD during the discharge period. I think Qmaxpassed Q goes from 0 to 10590mAh while Fcc was around 10738 during the all discharge cycle. 

But after the first ocv value is taken qmaxpassed Q updates to 0 and both DOD0 and QMAXDOD0 change from 0 to 16167mAh. I don't understand where such a high value comes from. 

Nevertheless, VOK clears properly as the discharge ends.

Here is a log of the discharge cycle of the learning cycle and a .gg file.

Could you please advise me?

Thanksfully, 

Paul ROCHE

learning cycle étape2 update stat=6.log030621.gg.csv